你好
我们在使用PCMD3180外接PDM麦克风,使用96Khz采样,信源为40khz的超声信号;分析采集结果发现严重失真,没有40khz。
如下fig_1,直接使用PDM麦克风采集40khz的超声信号,所得波形;
如下fig_2,使用PDM麦克风和PCMD3180,TDM接口协议,采样率96Khz,采集40khz的超声信号,所得波形;
手册表示可以采集80khz以内的信号,请问当前应该如何采集到40khz超声信号呢?
fig_1:
fig_2:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
采集20k的信号,结果正常
现在我们按照如下寄存器配置:
i2cset -f -y 1 0x4c 0x00 0x00
i2cset -f -y 1 0x4c 0x02 0x81
i2cset -f -y 1 0x4c 0x6b 0x05
i2cset -f -y 1 0x4c 0x07 0x30
i2cset -f -y 1 0x4c 0x3C 0x40
i2cset -f -y 1 0x4c 0x22 0x41
i2cset -f -y 1 0x4c 0x2B 0x45
i2cset -f -y 1 0x4c 0x73 0xC0
i2cset -f -y 1 0x4c 0x74 0xC0
i2cset -f -y 1 0x4c 0x75 0x60
采集40k信号,结果如下图:
可以采集到,但是对比我昨天发的fig_1,两个麦克风的包络有问题(形变)