TI工程师你好!
请帮忙确认一下TAS2505-Q1的电流参数谢谢!我提供外部的5V供电,IOVDD使用3.3V供电(IIC,IIS使用3.3V)Ityp是常规电源电流,Imax是最大电流。请帮忙确认两个参数电流值。我在芯片手册上没有发现该参数,谢谢。接一个4欧2.5W喇叭。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TI工程师你好!
请帮忙确认一下TAS2505-Q1的电流参数谢谢!我提供外部的5V供电,IOVDD使用3.3V供电(IIC,IIS使用3.3V)Ityp是常规电源电流,Imax是最大电流。请帮忙确认两个参数电流值。我在芯片手册上没有发现该参数,谢谢。接一个4欧2.5W喇叭。
您好,
您可以参考下面手册 2.5.3 Speaker output Power Consumption部分 中各电源的功耗,它提供的也是4欧姆喇叭下的功耗,但是SPKVDD 供电电压是3.6V,不过您可以根据P=UI进行换算,比如iSVDD为 功耗为 28.51mW,可以根据5V供电电压计算出对应的电流是 28.51mW/5=5.7mA。
表格中的功耗是测量出来的,如上面所述:All measurements were taken with the PLL turned off, no signal is present, and the DAC modulator is fully running.
下面E2E论坛帖子问题与您的类似,请参考帖子中TI工程师的回复: