This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA1656: 双电源±15V供电,同相放大2倍,负电压下不去

Part Number: OPA1656

使用运放放大,放大倍数2倍,后级空载接示波器测试,当输入是0V-3V可正常放大到0-6V,当输入为0V--3V,发现输出被限制在-2V。发现在-0.5V放大两倍还是正常的,低于-1V就无法超过-2V。信号就是DAC的直流电平。

  • 您好,

    这个电路这样接是没问题的,您是使用±15V供电吗?您可以实测下供电电压是否为期望的值?

    您可以用示波器同时测量输入和输出信号吗,让输入和输出信号显示在同一示波器屏幕中,截图附在这里,我想具体看下输入和输出信号是怎样的

  • 您好,您的问题解决了吗?如果还没有解决,您可以反馈我上面回复中的信息吗