This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM1808: PCM1808增益?

Part Number: PCM1808

PCM1808左右通道的增益是否为固定的99DB不可调节?客户的信号比较大,如果采用

PCM1808就会放大到很大,如果想要PCM1808得需要把输入信号处理得很小,这样误差会很大,是否有对增益的其它设置说明?

  • 您好,

    PCM1808没有增益调节模块,它的正常增益是1。您是在哪里看到 PCM1808左右通道的增益为99DB?或者说在PCM1808前级是否有增益电路放大了输入信号使得您误以为是PCM1808的增益?

  • PCM1808正常使用左右通道增益是多少呀?

    我看介绍是99DB呢

  • 这里写的是ADC SNR( Signal Noise Rate)典型值为99 dB,不是通道的增益。

    PCM1808没有增益调节电路,有的话数据手册中会进行说明的。

x 出现错误。请重试或与管理员联系。