This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM6360-Q1: 是否支持的TDM8格式

Part Number: PCM6360-Q1

你好

我在TDM 接口设计的时候希望和TAS6424E共用一条FS/BCLK接到DSP,TAS6424E配置为TDM8 48K,PCM6360是否也支持同样的配置 ?

感谢

  • 您好,

    在数据手册的表3 下方有一句话:The number of bit clock cycles in a frame must accommodate multiple device active output channels with the programmed data word length. 即一帧中的时钟周期数必须适应多个设备使能的输出通道数与字长。

    我不确定一帧中的时钟周期数必须等于输出通道数与字长的乘积,还是说可以大于输出通道数与字长的乘积。因为 PCM6360-Q1是6通道ADC,6个通道全部输出,是占6个slot;而TDM8 是8个slot。如果一帧中的时钟周期数必须等于输出通道数与字长的乘积,那么PCM6360就不支持TDM8 配置。这个问题待我确定后,我会在这里答复您

  • 那句话的意思是说BCLK 必须有足够的周期数来支持帧中的多个通道,具体取决于字长。也就是说另外2个slot可以为空,因此PCM6360可以支持TDM8 配置