This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AIC3254 I2S多个音频数据源同时接入

Other Parts Discussed in Thread: CC8530, TLV320AIC3254

我们的应用需要AIC3254 I2S接入TAS1020B来的双向I2S数据,以及同时双向接入4声道(2对立体声)的无线音频芯片CC8530。AIC3254同时接入模拟MIC,做Mixer处理,模拟音频输出到音箱和耳机。我们从GDE(PurePath Studio MiniDSP5.95)中看到AIC3254 I2S可以接入最多12个声道数据(I2S_6x_In组件)。不知道我们这个应用,AIC3254 I2S能否这样用?如果能,硬件上I2S ,CC8530和TAS1020B怎样连接AIC3254?PurePath Studio中又如何设置?谢谢!

  • 你好:

          TLV320AIC3254只有一路I2S,所有接收一路I2S。虽然它有primary I2S和Secondary I2S,但是它并不能同时使用,根据你的应用要求需要多路的I2S同时接收。所以AIC3254可能无法满足你的要求,建议选用可以支持多路I2S的codec如AIC3262,可支持3路I2S。你所见到的I2S_6X_In并不是可以接收6路I2S,而是指一帧I2S所接收的数据的个数。

  • Derek Xie,你好,我现在需要用到I2S_6X_In or Out的单个I2S接口接收和发送多个数据(一帧中),但是使用pps编译很多错误,你能帮我解决一下吗?

    问题描述在:http://www.deyisupport.com/question_answer/analog/audio/f/42/t/120298.aspx

  • 可以帮忙发个 

     PurePath™ Studio 图形开发环境  
      邮箱 252408976@qq.com