This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AIC3254的miniDSP问题



问题:AIC3254的miniDSP编写代码和编写C5502代码有什么区别,执行速度和代码量来进行分析吧,谢谢回复

  • 据我所知,AIC3254只能够使用TI提供的puth图形编程软件编写程序,还不支持自定义算法。只能使用软件中附带的控件来组合算法。可以这么认为,AIC3254是由第三方控制的miniDSP,算法和控制程序并不是烧写在AIC3254中,而是烧写在第三方控制器里面,再由控制器写入AIC3254中进行控制。和CC5502没有可比性

  • 问一个另外问题:miniDSP 中,I2S_OUT ,DOUT输出端数据波形是什么?与MonoI2S_OUT 有什么区别?

    相关文档上只解释了I2S_OUT,先是左声道16bit数据,然后是右声道16bit数据。但对MonoI2S_OUT呢?数据量减少一半?

    谢谢!

  • 你好:

               如果是I2S_OUT你的理解没错,先是左声道后是右声道,但是如果是MonoI2S_OUT输出的数据格式与I2S_OUT一致,只是数据只出现在一个声道。