Part Number: TAS6422E-Q1
你好,关于TAS6422E-Q有几个问题想咨询下:
- 规格书中这个I2C地址的时间怎么理解?

- 诊断功能是实时的吗?负载扬声器在播放,突然负载开路这种情况,可实时诊断吗?
- MUTE脚可以通过I2C控制,硬件外围也预留了控制;为了防止POPO声,上下电的时候需要满足如下的时序要求吗: PVDD->DVDD->STANDBY->UNMUTE
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TAS6422E-Q1
你好,关于TAS6422E-Q有几个问题想咨询下:

规格书中这个I2C地址的时间怎么理解?
I 2C ADDR1和I 2C ADDR0这两个引脚的高低电平决定了TAS6422的4种不同的从机地址。
所以当我们给这两个引脚高低电平的时候,也就是配置I2C地址的时候,到配置完成有个delay为300us。
诊断功能是实时的吗?负载扬声器在播放,突然负载开路这种情况,可实时诊断吗?
也是有一定诊断时间或者延迟的,在数据手册的电气参数表中都有给出,比如检测到输出被钳位,到诊断的时间不超过20us。

关于上掉电顺序,数据手册P20也由给出,VBAT和PVDD可以同时上电,VDD后于VBAT 和 PVDD再上电即可。

您好,mute和standby的区别在于, mute是使得输出为高阻态。standby是disable 内部大多数模拟电路然后使得器件处于低功耗状态节约功耗。对于TAS6422E的上掉电时序来说,按照上述datasheet中的上掉电顺序就好。
如果上掉电从系统级来看的话,先给系统上电,再给TAS6422E上电,掉电时候,先给TAS6422E掉电,系统再掉电,这也是预防开关机POP声的办法。
嗯明白您的意思,但是对于TAS6424来说,mute和standby没有这个时序要求,如果有的话,数据手册中都会有给出具体要求,所以即使在上电之前,/STANDBY = 0 & MUTE = 1 或者STANDBY = 1 & MUTE = 0都是可以的。