Part Number: TAS5766M
TAS5766遇到一些问题 ,请能帮忙解决。
1, 正常情况,不加EQ时,用DC15V供电4欧姆负载,喇叭端输出最大有9V左右开始有失真。

2,当加了EQ,其它条件相同,喇叭端输出最大2V多就会失真,用DEMO板测试的。这一定是有问题的,请帮忙看一下怎么解决?


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,通过第一个图可以看出,当输出为9V时,输出波形开始削波,输出达到饱和。输入是+-1V的信号是吗,gain设置的多少?输出是否有加滤波电路?输出波形是否是在TAS5766的输出端测试的还是在经过filter之后的波形?
另外,加上EQ之后,2V左右就开始失真,您是如何配置的EQ?
前面第一幅图DC15V供电,4欧姆负载,最大不失真(1%失真)输出9.2V(约21W),是正常的。这个是作为说明第二幅图参数异常的参考。
第二幅图,设定好EQ后,最大不失真(1%失真)输出只有2.5V左右(约1.5W),声音不正常了(输入500HZ,800mV正弦波形)。
EQ设定的PPC3文件(PPC3文件上传不了,是否可以提供您的个人邮箱,我邮件给您)和CFG文件请参考附件。