This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5719: 功放过载问题

Part Number: TAS5719


我们在使用TAS5719的时候,发现不同的批次表现不一样,这一个批次的都正常,下一个批次的有过载的问题.

原理图如下PDF文件:

TPS5719.pdf

软件设置如下:

/* 5719初始化数据 */
{0x1B, 1, {0x00}},      /*Oscillator trim register振荡器调整寄存器*/
{0x1B, 1, {0x00}},
{0x03, 1, {0x80}},      /*System control register 1*/
{0x11, 1, {0x77}},      /*IC delay channel 1*/
{0x12, 1, {0x7F}},      /*IC delay channel 2*/
{0x13, 1, {0x77}},      /*IC delay channel 3*/
{0x14, 1, {0x7F}},      /*IC delay channel 4*/
{0x1C, 1, {0x07}},      /*BKND_ERR register*/
{0x0A, 1, {0x30}},      /*Channel 3 vol*/
{0x0E, 1, {0xF1}},      /*Volume configuration register音量寄存器*/
{0x00, 1, {0x6C}},      /*Clock control register*/
{0x50, 4, {0x0F, 0x70, 0x80, 0x10}},        /*EQ control*/
{0x25, 4, {0x01, 0x02, 0x13, 0x45}},        /*PWM MUX register*/
{0x70, 4, {0x00, 0x80, 0x00, 0x00}},        /*ch1 inline mixer*/
{0x71, 4, {0x00, 0x00, 0x00, 0x00}},        /*inline_DRC_en_mixer_ch1*/
{0x74, 4, {0x00, 0x80, 0x00, 0x00}},        /*ch2 inline mixer*/
{0x75, 4, {0x00, 0x00, 0x00, 0x00}},        /*inline_DRC_en_mixer_ch2*/
//{0x46, 4, {0x00, 0x02, 0x06, 0x23}},        /*DRC control*/
{0x46, 4, {0x00, 0x02, 0x06, 0x20}},        /*DRC control*/ //DRC off
{0x05, 1, {0x00}},                          /*System control register 2*/
{0x08, 2, {0x00, 0xC0}},
{0x09, 2, {0x00, 0xC0}},
{0x56, 4, {0x00, 0x40, 0x00, 0x00}},        /*Output post-scale*/
{0x57, 4, {0x00, 0x02, 0x00, 0x00}},        /*Output pre-scale*/
{0x07, 2, {0x00, 0x72}},
{0x07, 2, {0x03, 0xFF}},                    /*Master volume,关音了*/
//{0x0B, 2, {0x01, 0x80}},/* 耳机音量 -3Db*/

//EQ
 {0x27, 20,  {0x00, 0x7F, 0xAA, 0x6F, 0x0F, 0x80, 0x55, 0x91, 0x00, 0x00, 0x00, 0x00, 0x00, 0x7F, 0x54, 0xDF, 0x00, 0x00, 0x00, 0x00}},
 {0x28, 20,  {0x00, 0x80, 0x7C, 0x93, 0x0F, 0x01, 0x43, 0x46, 0x00, 0x7E, 0x43, 0x4B, 0x00, 0xFE, 0xBC, 0xBA, 0x0F, 0x81, 0x40, 0x22}},
 {0x29, 20,  {0x00, 0x77, 0x81, 0xB2, 0x0F, 0x35, 0xE9, 0x9C, 0x00, 0x5A, 0x76, 0xD2, 0x00, 0xCA, 0x16, 0x64, 0x0F, 0xAE, 0x07, 0x7C}},
 {0x2A, 20,  {0x00, 0xBE, 0x7D, 0x93, 0x0E, 0xE0, 0x31, 0xCA, 0x00, 0x73, 0xFE, 0x1A, 0x00, 0xB2, 0x25, 0x87, 0x0F, 0xBB, 0x2D, 0x02}},
 {0x2B