This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM1864: 从master模式调整为slave模式音频无法采集

Part Number: PCM1864

您好:

       之前我们已经实现了PCM1864做主模式的调试并完成了生产,先有芯片做从的需求需要实现,调试更改后还没有音频输出,需要提示一下在从主模式到从模式硬件和软件需要更改的地方,原理图及已经尝试方法如下

   

此原理图已实现芯片做主,做主配置如下

i2c_write 0 0x96 0 0
i2c_write 0 0x96 0x06 0x01
i2c_write 0 0x96 0x07 0x01
i2c_write 0 0x96 0x08 0x02
i2c_write 0 0x96 0x09 0x02
i2c_write 0 0x96 0x0B 0xCF
i2c_write 0 0x96 0x0A 0x00
i2c_write 0 0x96 0x0C 0x01
i2c_write 0 0x96 0x26 0x01
i2c_write 0 0x96 0x27 0xFF
i2c_write 0 0x96 0x20 0x91
i2c_write 0 0x96 0x19 0x0f
i2c_write 0 0x96 0x03 0xe8
尝试芯片做从模式: 1.修改芯片主从模式 i2c_write 0 0x96 0x20 0x01  #没有音频录制
                                 2.去掉外部晶振x7                                                   #没有音频录制
                                 3.修改BCLK给到芯片2Mhz、6Mhz、12Mhz          #没有音频录制
目前状态SCKI引脚12.288
               LRCK      48Khz
               
i2c_write 0 0x96 0 0
i2c_write 0 0x96 0x06 0x01
i2c_write 0 0x96 0x07 0x01
i2c_write 0 0x96 0x08 0x02
i2c_write 0 0x96 0x09 0x02
i2c_write 0 0x96 0x0B 0xCF
i2c_write 0 0x96 0x0A 0x00
i2c_write 0 0x96 0x0C 0x01
i2c_write 0 0x96 0x26 0x01
i2c_write 0 0x96 0x27 0xFF
i2c_write 0 0x96 0x20 0x01
i2c_write 0 0x96 0x19 0x0f
i2c_write 0 0x96 0x03 0xe8