Part Number: TPA3116D2
只有1片,
Master
SYNC 如何接呢?
我现在是串4.7K和47pF 到地
INPR 串 1.0uF+51K
INPL 串 1.0uF+51K
Gain 47K 75K 36dB
电源是11V,4R 喇叭 声音不大
Power GND 需要接散热片接到GND 吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
Master模式下SYNC 管脚是输出状态,可以悬空;
不建议串51K电阻,如下输入阻抗电路,串联51K电阻会降低 TPA3116D2内部设置的增益:

另外,输入电容和输入阻抗会形成高通滤波器,请根据数据手册7.3.2 Input Impedance部分设置合适的输入电容:

声音不大,有可能是 输入电容和串联输入电阻 降低电路增益造成的,另外注意PLIMIT管脚的设置电压是限制输出功率,检查下PLIMIT管脚电压是否限制了输出功率。
为了更好的噪声性能,建议将散热器接地、Power GND接地。