This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM5100A: PCM5100A输出失真问题

Part Number: PCM5100A


各位好,最近测试遇到一个问题。

使用S32K144调用Nor Flash里的一个1KHz的BIN文件,再通过PCM5100A(DAC)+TAS5411(功放)播放出来,测量其失真(TAS5411输出)为1.5%,测量PCM5100A的输出,失真也为1.5%左右。

而如果是使用外部信号发生器直接从PCM5100A的输出端处输入1KHz信号,测量其失真则为0.22%,所以后级电路是没有问题的。

我们现在怀疑:1、5100A的输出失真就是那么高;2是MCU的bin文件解码能力有问题

请问有什么办法可以排除5100A的问题?

下图分别是调用Flash的输出失真,信号发生器输出失真,以及PCM5100A的原理图。