This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320ADC3101: 基准和转化公式

Part Number: TLV320ADC3101


Dears:

  我想用TLV320ADC3101做AD转换,请问其基准和转化公式是怎样的呢?

  • 您好,

    该器件的测量范围是以1.35V为中心(共模电压1.35V)有效幅值0.707Vrms,即 0.35V至2.35V。0.35V直流输入将产生最大负代码0x80000000,同样2.35V直流将产生最大正输出代码7FFFFFFF,请注意这里会存在一定的增益误差和偏移。如果您尝试计算输入的模拟电压,您需要将输出的2的补码格式转换为十进制数,然后可以使用下面公式计算输入电压:

     (CODE/2^31)/PGAGain + 1.35V.