This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5805M: Electrical Characteristics標示說明

Part Number: TAS5805M
Other Parts Discussed in Thread: TPS61230,

一般零件(如LDO, Buck, Boost等),如TPS61230 Datasheet的項目Electrical Characteristics會標示"TJ = –40°C to 125°C and VIN = 3.6 V. Typical values are at TJ = 25°C, unless otherwise noted.",

但為什麼Speaker AMP的Electrical Characteristics通常只標"室溫規格",比如TAS5805M的項目Electrical Characteristics,標示Free-air room temperature 25°C (unless otherwise noted),而未含概高溫、低溫

  • 您好,大多数器件的电气参数基本上都是在室温25测试得到的结果。像TAS5805M也是。

    您提到TPS61230的电气参数表中,我看下了下, 典型值也都是在25度下测试得到的。 其他范围值应该是在TJ = –40°C to 125°C范围内测量的结果。

    具体LDO的电气参数表中,最小和最大值是否针对最低温和最高温对应的值,建议您在“电源管理”论坛和电源工程师确认下。

    像我遇到的大多数器件的电气参数是针对室温测试的,然后会有不同电气参数随着温度变化的温漂系数。

    不同器件的规格应该是不同的,所以建议您和电源工程师确认。

  • 謝謝您的回覆!

    希望會有TI音頻的工程師,能幫忙對TAS5805M做出回覆,為何項目Electrical Characteristics,只標示Free-air room temperature 25°C,而不像TPS61230的項目Electrical Characteristics會標示"TJ = –40°C to 125°C 

  • 只标示Free-air room temperature 25°C的意思是,下面表格的电气参数都是在25度下测试的。

    您是需要知道其他温度的具体某个参数值吗?