This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC23B: 求助aic23b从模式AD/DA问题

Part Number: TLV320AIC23B


MCLK选用12.288Mhz 模式SLAVE 数字接口 I2S  

BCLK:12.288Mhz 采样率:96khz   BIT = 16bit

mic输入 旁路模式下 能够清楚听到输入的音频 。

主要问题:关闭旁路切到I2S模式后 通过I2S接口发现读取AD数据一直为高电平 。I2S接口发送噪声信号耳机无任何声音。

请教:有没有什么解决方法和解决思路,该如何验证芯片内部ad和da正常工作

I2S接口使用示波器看过和期望的一致。

寄存器通过配置旁路可以验证寄存器能够进行正确的配置。

寄存器配置流程如下:

addr:0x0f value:0x0

addr:0x0f value:0x1

addr:0x08 value:0x0

addr:0x07 value:0x12

addr:0x09 value:0x1

addr:0x00 value:0x17

addr:0x01 value:0x17

addr:0x02 value:0x7f

addr:0x03 value:0x7f

addr:0x04 value:0x15

addr:0x05 value:0x06

addr:0x06 value:0x01