This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC23B: TLV320AIC23BPW,ADC, Analog Line Input转I2S输出,波形失真

Part Number: TLV320AIC23B


项目采用TLV320AIC23BPW进行ADC转换,通过Line输入,转成I2S输出给FPGA转成并行数据,寄存器配置成主模式,外部用12M晶振,采样率为32K。

输入1K的正弦波,在1.0Vrms范围内,FPGA转成的并行数据绘制波形如下图所示:

调相关寄存器,最多影响最高点和最低点的幅度,还是没法恢复正弦波。

通过TLV320AIC23BPW进行ADC-DAC转换,用示波器测试DA转换是正弦波。

硬件设计图如下:

寄存器配置如下:

寄存器先配置的复位寄存器,尝试过别的采样率和从模式18.432,绘制的波形差不多,实在找不出问题可能出在哪里,请大神赐教!