Other Parts Discussed in Thread: PCM1808, PCM1808EVM, PCM1753, PCM1754, DRV632, PCM3168A, SA5532
您好:
我最近在做一个多路语音切换的项目(其中包含两路语音叠加后从另一路输出),采用的方案是ADC+FPGA+DAC。ADC我选的是PCM1808,DAC选的是PCM1753,均采用左对齐方式。PCM1808的手册中说输入的模拟电压极限范围是-0.3V to (VCC+0.3V),实际的输入范围应该是1V-4V(以2.5V为中心,幅度3Vpp),但是在PCM1808EVM中,模拟信号进入PCM1808之前加了一个大电容,隔去了直流成分,变为了正负信号。我想问的是,是不是不管音频信号的直流电平是多少,只要加一个大的电容,即可接入PCM1808,而不必利用搬移电路将直流搬移到+2.5V。