Other Parts Discussed in Thread: TLV320AIC3254
根据TIBQ软件工具可以计算EQ系数
Text "* Sample Rate = 44100"
Text "* Filter 1 EQ 21 Hz Fc 8.0 dB 4 Hz BW"
Text "* H(z) = (N0 + 2*N1/z + N2/(z2)) / (32768 - 2*D1/z - D2/(z2))"
Text "* Filter Coefficients in format N0, N1, N2, D1, D2"
Text "* Filter 1"
0x7FFFFF
0x8018AF
0x7FCEEF
0x7FF60C
0x80139C
我的问题是H(z) = (N0 + 2*N1/z + N2/(z2)) / (32768 - 2*D1/z - D2/(z2))"这个公式是怎样计算出 N0, N1, N2, D1, D2"的,只能通过这个软件才能计算吗?我想在手机中应用这个EQ,用嵌入式软件产生 N0, N1, N2, D1, D2,好写入3254中,请教等待中