Part Number: PCM6240-Q1
Hello,
请问一下,关于PCM6240 AC-Coupled Single-Ended Input Connection中,偏置电阻R0的作用是将INP和INM偏置到合适的Common-mode Voltage:
- 这个Common-mode Voltage的作用是什么
- 如果设计中没有这个偏置电阻会有何影响;

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: PCM6240-Q1
Hello,
请问一下,关于PCM6240 AC-Coupled Single-Ended Input Connection中,偏置电阻R0的作用是将INP和INM偏置到合适的Common-mode Voltage:

您好,
1、看下面 PCM6240内部框图截图,INXP和INXM连接的是衰减器和PGA,衰减器或PGA有输入共模电压要求,因此为了满足输入信号的最大摆幅,输入信号需满足内部衰减器或PGA的输入共模电压要求,这里的Common-mode Voltage的作用就是用来使输入信号满足其输入共模电压要求的以达到最大输入信号范围。

2、没有这个偏置电阻是指不设置输入信号的共模电压吗?如果是这样的话,输入信号可能会超出上述衰减器或PGA输入信号范围,导致信号失真或削顶。
datasheet 如下截图部分,点击蓝色字体可以下载外部电阻计算工具,或见下面附件

感谢回复,以下几点再帮忙确认一下:
(1) 共模电压的根本作用是否是将输入信号抬升到0.1 ~ (MICBIAS-0.1)范围内?
(2) PCM6xx0-Q1 AC Coupled External Resistor Calculator文档有查看过,看到PCM6xx0的INP和INM内部结构如下图所示,这是否为一个全差分放大器,全差分放大器内部是否已经有一个Vocm?

(3) 目前我们在应用的过程中,是按照MIC的DATASHEET的建议设计电路,MIC的信号接AC耦合电容到INP,INM直接接到GND,但软件配置的PCM6240寄存器用的是DC-Coupled方式;已经实测该电路,MIC录音回放效果声音比较清晰,没有出现失真的现象,但不确定这种使用方法是否有潜在的问题;


已经实测该电路,MIC录音回放效果声音比较清晰,没有出现失真的现象,
很抱歉回复这么晚,您这里应用的MIC输出摆幅范围是多少?这里建议您INXP管脚外部加直流偏置,确保输入信号符合PCM6240输入范围,如下红色框内电路: