This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如题,在使用aic3254开发板时希望可以脱离pc上的软件实现对3254的控制,即直接使用keil下载程序到1020b中控制3254。目前已经实现了调用rom中的i2c函数写入3254的配置系数,那么如果要使用usb传输控制命令应该怎么做?
因为在使用tas1020b firmware development kit 中的v1.8程序时,发现下载以后在计算机管理里面显示的是unknow device,是不是v1.8中的application程序有问题?要如何更改?目前希望做到的是将application程序修改,使得其效果跟usb-miniEVM0203_441KHZ.BIN下载进去一样,即AIC3254CS 软件能够识别和操作。
因为development kit 中的tsc2100_FW8程序是能够运行并被计算机识别为声音和usb设备的,因而application程序应该也具有相同的功能吧。
或者,usb-miniEVM0203_441khz.bin的程序能不能看一下?
期待您的回复!
(ps:这个帖子之前发在其他DSP & ARM® 产品 分类下,无人回复,希望在这里得到解答。)