Other Parts Discussed in Thread: TAS5721
TAS5721使用的时候为什么需要拉低一下才有声音输出?其它的产品我记得,PDN不用接都没有问题的?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TAS5721
TAS5721使用的时候为什么需要拉低一下才有声音输出?其它的产品我记得,PDN不用接都没有问题的?
TAS5721初始化过程中并不需要拉低PND。初始化过程:
1. Hold all digital inputs low and ramp up AVDD/DVDD to at least 3 V.
2. Initialize digital inputs and PVDD supply as follows:
• Drive RST = 0, PDN = 1, and other digital inputs to their desired state while ensuring that all
are never more than 2.5 V above AVDD/DVDD. Wait at least 100 μs, drive RST = 1, and wait
at least another 13.5 ms.
• Ramp up PVDD to at least 8 V while ensuring that it remains below 6 V for at least 100 μs
after AVDD/DVDD reaches 3 V. Then wait at least another 10 μs.
3. Trim oscillator (write 0x00 to register 0x1B) and wait at least 50 ms.
4. Configure the DAP via I2C (see Users's Guide for typical values).
5. Configure remaining registers.
6. Exit shutdown (sequence defined below).
Exit shutdown:
1. Write 0x00 to register 0x05 (exit shutdown command may not be serviced for as much as 240 ms
after trim following AVDD/DVDD powerup ramp).
2. Wait at least 1 ms + 1.3 × tstart (where tstart is 300 ms when mid-Z ramp is enabled and is
otherwise specified by register 0x1A).
3. Proceed with normal operation
请检查您是否正确按照顺序编程