如果TAS57XX系列没有MCLK输入,需要怎么样去设置寄存器,另外MCLK脚是应该悬空,还是其他怎么样设置!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如果TAS57XX系列没有MCLK输入,需要怎么样去设置寄存器,另外MCLK脚是应该悬空,还是其他怎么样设置!
你好,
TAS57xx工作时必须要有MCLK,若主芯片无MCLK输出,可以将主芯片的BCLK同时作为MCLK给TAS57xx,但要求是Fs必须为44.1kHz或48kHz,BCLK必须为64*Fs。
谢谢!
jacky:
您好!
那0X00寄存器是否需要更改设置 ,默认是256.Fs
问下,是所有的TAS57XX都 可以这么用吗?还是只能5709用,这样用会有什么影响吗?