This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于TPA3118 保护及恢复问题

你好!

       最近在使用TPA3118应用于车载项目,有如下问题请教:

       在TPA3118规格书第18页表4中,前三种错误(over current/over temperature/ too high DC Offset) 发生后,要如何恢复?由于TPA3118 PVCC直接连接在车身B+上,不可能通过PVCC通断来恢复。

       谢谢!

 

 

  • 你好:

           并不是所有的保护都需要PVCC通断的,只有DC detection才需要通断PVCC。这种情况下,说明电路有错误,需要检修了。

  • 1. DC Detection是否会在音频输入信号建立的过程中容易产生?之前发生过 音频处理器因故障复位,导致TPA3118无声的情况发生,只有通过断电才能恢复。

    2. 输出信号+/-短路是否可以自行恢复?

    3.在车载应用中,PVCC是否需要加一个开关?

    谢谢!

  • 你好:

    1.音频输入信号建立的过程中不容易产生。我的理解音频信号的建立就是慢慢的将信号的声音放大,音乐存在直流成分的概率很小。

    2.输出信号短路可以自行恢复。

    3.你的PVCC的源是从哪里来的?

  • 1.音频耦合电容建议不要用电解电容。这样直流检测功能一般不会误触发。

    2。温度过高和输出短路可以在温度降低,短路解除后自行恢复。

    3。车载设备加开关不太现实吧。一般车载功放电源都是长接蓄电池正极的。当然也可以接点火开关后,不过基本没这种设计。

    TI的功放只要工作在待机模式状态,功耗是很小的。(应该小于0.1W,建议你自己测试一下。我以前用的TPA3110整机待机功耗就在0.2W左右。)