Other Parts Discussed in Thread: PCM4220, PCM1792A
请问PCM4220数据手册中给的群延时时间和数字滤波器延时时间是同一个概念吗?手册中对于低群延时滤波器的响应是21个点,不过我实际测量会有一些差别,实际测试的结果是53或者54个点,对于经典滤波器手册中给的是39个点,实际测试是71或者72个点。选用的采样率为:26k,50k,100k,102.4k
我是这么测试的,用信号源产生一个0.1Hz的方波信号,脉宽为200ms,将这个方波分为两路,一路作为PCM4220采样数据的开始标志(此时PCM4220已经稳定运行一段时间,排除开始启动采集时的干扰),另一路作为实际的输入信号。当接收到开始标志时开始记数,到PCM4220输出的数据为方波信号的上升沿为止,实际测试的点数如上面所说,低群延时为53,经典为71。请问这个测试方法是否合理,发现我们测试的和手册中给出的两种滤波器相差点数是相同的,不过会差出30个采样点,请问这是什么情况。或者对于群延时这个指标,我们如何来验证一下