This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC23B MIC产生回音,求助!

Other Parts Discussed in Thread: TLV320AIC23B

我司用TLV320AIC23B设计,耳机在对讲时会有回音,经过测试发现MIC信号有干扰,单板测出正常,但是接上耳机会有0.9mVrms的电压,现在解决了串扰不失真,但是回音仍然存在,求指导!谢谢! 调试电阻电容是否会有改善?

  • MIC与耳机听筒距离是否距离较近,MICBIAS去耦电容C61去掉。MIC和耳机听筒是共用一个连接器吗?有无接触不良?

  • mic和耳机距离不近,板子到mic还有一根转接线连接的,不是普通那种pcb上接连接器那种。不是连接器不良,对了,那个mic的地我与板子上的大地都是连在一起的,也就是说并没有分agnd,dgnd. 这样回路会有很大影响吗?

  • 理论上讲会有一些影响,但不至于到产生回声这种级别。有没有换个耳机试试?

    另外方便的话把你完整的电路和PCB文件发上来看看。

  • 您的mic功能是怎么实现的呀???我这边改了部分程序内容还是没反应,是不是寄存器要改呀!!!下面是我改的程序,求指教!!!

    #include <csl.h>
    #include <csl_i2c.h>
    #include <stdio.h>
    #include <csl_pll.h>
    #include <csl_mcbsp.h>

    #define CODEC_ADDR 0x1A


    /*锁相环的设置*/
    PLL_Config myConfig = {
    0, //IAI: the PLL locks using the same process that was underway
    //before the idle mode was entered
    1, //IOB: If the PLL indicates a break in the phase lock,
    //it switches to its bypass mode and restarts the PLL phase-locking
    //sequence
    12, //PLL multiply value; multiply 24 times
    1 //Divide by 2 PLL divide value; it can be either PLL divide value
    //(when PLL is enabled), or Bypass-mode divide value
    //(PLL in bypass mode, if PLL multiply value is set to 1)
    };


    MCBSP_Config Mcbsptest;

    /*McBSP set,we use mcbsp1 to send and recieve the data between DSP and AIC23*/
    MCBSP_Config Mcbsp1Config = {
    MCBSP_SPCR1_RMK(
    MCBSP_SPCR1_DLB_OFF, /* DLB = 0,禁止自闭环方式 */
    MCBSP_SPCR1_RJUST_LZF, /* RJUST = 2 */
    MCBSP_SPCR1_CLKSTP_DISABLE, /* CLKSTP = 0 */
    MCBSP_SPCR1_DXENA_ON, /* DXENA = 1 */
    0, /* ABIS = 0 */
    MCBSP_SPCR1_RINTM_RRDY, /* RINTM = 0 */
    0, /* RSYNCER = 0 */
    MCBSP_SPCR1_RRST_DISABLE /* RRST = 0 */
    ),
    MCBSP_SPCR2_RMK(
    MCBSP_SPCR2_FREE_NO, /* FREE = 0 */
    MCBSP_SPCR2_SOFT_NO, /* SOFT = 0 */
    MCBSP_SPCR2_FRST_FSG, /* FRST = 0 */
    MCBSP_SPCR2_GRST_CLKG, /* GRST = 0 */
    MCBSP_SPCR2_XINTM_XRDY, /* XINTM = 0 */
    0, /* XSYNCER = N/A */
    MCBSP_SPCR2_XRST_DISABLE /* XRST = 0 */
    ),
    /*单数据相,接受数据长度为16位,每相2个数据*/
    MCBSP_RCR1_RMK(
    MCBSP_RCR1_RFRLEN1_OF(1), /* RFRLEN1 = 1 */
    MCBSP_RCR1_RWDLEN1_16BIT /* RWDLEN1 = 2 */
    ),
    MCBSP_RCR2_RMK(
    MCBSP_RCR2_RPHASE_SINGLE, /* RPHASE = 0 */
    MCBSP_RCR2_RFRLEN2_OF(0), /* RFRLEN2 = 0 */
    MCBSP_RCR2_RWDLEN2_8BIT, /* RWDLEN2 = 0 */
    MCBSP_RCR2_RCOMPAND_MSB, /* RCOMPAND = 0 */
    MCBSP_RCR2_RFIG_YES, /* RFIG = 0 */
    MCBSP_RCR2_RDATDLY_1BIT /* RDATDLY = 1 */
    ),
    MCBSP_XCR1_RMK(
    MCBSP_XCR1_XFRLEN1_OF(1), /* XFRLEN1 = 1 */
    MCBSP_XCR1_XWDLEN1_16BIT /* XWDLEN1 = 2 */

    ),
    MCBSP_XCR2_RMK(
    MCBSP_XCR2_XPHASE_SINGLE, /* XPHASE = 0 */
    MCBSP_XCR2_XFRLEN2_OF(0), /* XFRLEN2 = 0 */
    MCBSP_XCR2_XWDLEN2_8BIT, /* XWDLEN2 = 0 */
    MCBSP_XCR2_XCOMPAND_MSB, /* XCOMPAND = 0 */
    MCBSP_XCR2_XFIG_YES, /* XFIG = 0 */
    MCBSP_XCR2_XDATDLY_1BIT /* XDATDLY = 1 */
    ),
    MCBSP_SRGR1_DEFAULT,
    MCBSP_SRGR2_DEFAULT,
    MCBSP_MCR1_DEFAULT,
    MCBSP_MCR2_DEFAULT,
    MCBSP_PCR_RMK(
    MCBSP_PCR_IDLEEN_RESET, /* IDLEEN = 0 */
    MCBSP_PCR_XIOEN_SP, /* XIOEN = 0 */
    MCBSP_PCR_RIOEN_SP, /* RIOEN = 0 */
    MCBSP_PCR_FSXM_EXTERNAL, /* FSXM = 0 */
    MCBSP_PCR_FSRM_EXTERNAL, /* FSRM = 0 */
    0, /* DXSTAT = N/A */
    MCBSP_PCR_CLKXM_INPUT, /* CLKXM = 0 */
    MCBSP_PCR_CLKRM_INPUT, /* CLKRM = 0 */
    MCBSP_PCR_SCLKME_NO, /* SCLKME = 0 */
    MCBSP_PCR_FSXP_ACTIVEHIGH, /* FSXP = 0 */
    MCBSP_PCR_FSRP_ACTIVEHIGH, /* FSRP = 1 */
    MCBSP_PCR_CLKXP_FALLING, /* CLKXP = 1 */
    MCBSP_PCR_CLKRP_RISING /* CLKRP = 1 */
    ),
    MCBSP_RCERA_DEFAULT,
    MCBSP_RCERB_DEFAULT,
    MCBSP_RCERC_DEFAULT,
    MCBSP_RCERD_DEFAULT,
    MCBSP_RCERE_DEFAULT,
    MCBSP_RCERF_DEFAULT,
    MCBSP_RCERG_DEFAULT,
    MCBSP_RCERH_DEFAULT,
    MCBSP_XCERA_DEFAULT,
    MCBSP_XCERB_DEFAULT,
    MCBSP_XCERC_DEFAULT,
    MCBSP_XCERD_DEFAULT,
    MCBSP_XCERE_DEFAULT,
    MCBSP_XCERF_DEFAULT,
    MCBSP_XCERG_DEFAULT,
    MCBSP_XCERH_DEFAULT
    };
    /* This next struct shows how to use the I2C API */
    /* Create and initialize an I2C initialization structure */
    I2C_Setup I2Cinit = {
    0, /* 7 bit address mode */
    0, /* own address - don't care if master */
    84, /* clkout value (Mhz) */
    50, /* a number between 10 and 400*/
    0, /* number of bits/byte to be received or transmitted (8)*/
    0, /* DLB mode on*/
    1 /* FREE mode of operation on*/
    };

    I2C_Config testI2C;


    /*数字音频接口格式设置
    AIC23为主模式,数据为DSP模式,数据长度16位*/
    Uint16 digital_audio_inteface_format[2]={0x0e,0x53};
    /*AIC23的波特率设置,采样率为44.1K*/
    Uint16 sample_rate_control[2] = {0x10,0x20};
    /*AIC23寄存器复位*/
    Uint16 reset[2] ={0x1e,0x00};
    /*AIC23节电方式设置,所有部分均所与工作状态*/
    Uint16 power_down_control[2] ={0x0c,0x01};
    /*AIC23模拟音频的控制
    DAC使能,ADC输入选择为MIC*/
    Uint16 analog_aduio_path_control[2] ={0x08,0x15};
    /*AIC23数字音频通路的控制*/
    Uint16 digital_audio_path_control[2] ={0x0a,0x05};
    /*AIC23数字接口的激活*/
    Uint16 digital_interface_activation[2] ={0x12,0x01};
    /*AIC23左通路音频调节*/
    Uint16 left_line_input_volume_control[2] ={0x00,0x00};
    /*AIC23右通路音频调节*/
    Uint16 right_line_input_volume_control[2] ={0x02,0x00};
    /*AIC23耳机左通路音频调节*/
    Uint16 left_headphone_volume_control[2] ={0x05,0x79};
    /*AIC23耳机右通路音频调节*/
    Uint16 right_headphone_volume_control[2] = {0x07,0x79};
    /*定义McBSP的句柄*/
    MCBSP_Handle hMcbsp;

    Uint16 i2c_status;
    Uint16 i,temp;

    void delay(Uint32 k)
    {
    while(k--);
    }


    void main(void)
    {

    Uint16 aic23data = 0;
    i2c_status = 1;
    /* Initialize CSL library - This is REQUIRED !!! */
    /*初始化CSL库*/
    CSL_init();

    /*设置系统的运行速度为140MHz*/
    PLL_config(&myConfig);

    /* Initialize I2C, using parameters in init structure */
    /*初始化I2C的格式*/

    // I2C_config(&Config);
    // I2C_start();

    // I2C_getConfig(&Config1);
    /*I2C is undet reset*/
    I2C_RSET(I2CMDR,0);
    /*设置预分频寄存器,I2C的mode clock is 10MHz*/
    delay(100);
    I2C_RSET(I2CSAR,0x001A);

    I2C_RSET(I2CMDR,0x0620);

    I2C_setup(&I2Cinit);
    /*设置I2C的Mater clock*/
    I2C_RSET(I2CCLKL,100);

    I2C_RSET(I2CCLKH,100);

    I2C_getConfig(&testI2C);

    /*初始化McBSP0*/
    hMcbsp = MCBSP_open(MCBSP_PORT0,MCBSP_OPEN_RESET);
    /*设置McBSP0*/
    MCBSP_config(hMcbsp,&Mcbsp1Config);
    /*启动McBSP0*/
    MCBSP_start(hMcbsp,
    MCBSP_RCV_START | MCBSP_XMIT_START,
    0);

    MCBSP_getConfig(hMcbsp,&Mcbsptest);

    /*reset AIC23*/
    i2c_status = I2C_write( reset, //pointer to data array
    2, //length of data to be transmitted
    1, //master or slaver--master
    CODEC_ADDR, //slave address to transmit to
    1, //transfer mode of operation
    30000 //time out for bus busy
    );
    delay(1000);
    /*设置AIC23各部分均工作*/
    i2c_status = I2C_write( power_down_control,//pointer to data array
    2, //length of data to be transmitted
    1, //master or slaver
    CODEC_ADDR, //slave address to transmit to
    1, //transfer mode of operation
    30000 //time out for bus busy
    );
    /*设置AIC23的数字接口*/
    i2c_status = I2C_write( digital_audio_inteface_format,//pointer to data array
    2, //length of data to be transmitted
    1, //master or slaver
    CODEC_ADDR, //slave address to transmit to
    1, //transfer mode of operation
    30000 //time out for bus busy
    );
    /*设置AIC23模拟通路*/
    i2c_status = I2C_write( analog_aduio_path_control,//pointer to data array
    2, //length of data to be transmitted
    1, //master or slaver
    CODEC_ADDR, //slave address to transmit to
    1, //transfer mode of operation
    30000 //time out for bus busy
    );
    /*设置数字通路*/
    i2c_status = I2C_write( digital_audio_path_control,//pointer to data array
    2, //length of data to be transmitted
    1, //master or slaver
    CODEC_ADDR, //slave address to transmit to
    1, //transfer mode of operation
    30000 //time out for bus busy
    );
    /*设置AIC23的采样率*/
    i2c_status = I2C_write( sample_rate_control,//pointer to data array
    2, //length of data to be transmitted
    1, //master or slaver
    CODEC_ADDR, //slave address to transmit to
    1, //transfer mode of operation
    30000 //time out for bus busy
    );
    /*设置耳机音量*/
    i2c_status = I2C_write( left_headphone_volume_control,//pointer to data array
    2, //length of data to be transmitted
    1, //master or slaver
    CODEC_ADDR, //slave address to transmit to
    1, //transfer mode of operation
    30000 //time out for bus busy
    );
    i2c_status = I2C_write( right_headphone_volume_control,//pointer to data array
    2, //length of data to be transmitted
    1, //master or slaver
    CODEC_ADDR, //slave address to transmit to
    1, //transfer mode of operation
    30000 //time out for bus busy
    );
    /*设置Line输入的音量*/
    i2c_status = I2C_write( left_line_input_volume_control,//pointer to data array
    2, //length of data to be transmitted
    1, //master or slaver
    CODEC_ADDR, //slave address to transmit to
    1, //transfer mode of operation
    30000 //time out for bus busy
    );
    i2c_status = I2C_write( right_line_input_volume_control,//pointer to data array
    2, //length of data to be transmitted
    1, //master or slaver
    CODEC_ADDR, //slave address to transmit to
    1, //transfer mode of operation
    30000 //time out for bus busy
    );
    /*启动AIC23*/
    i2c_status = I2C_write( digital_interface_activation,//pointer to data array
    2, //length of data to be transmitted
    1, //master or slaver
    CODEC_ADDR, //slave address to transmit to
    1, //transfer mode of operation
    30000 //time out for bus busy
    );

    /*回放音频*/
    while(TRUE)
    {
    while(!MCBSP_rrdy(hMcbsp)){};

    aic23data = MCBSP_read16(hMcbsp);

    // while(!MCBSP_xrdy(hMcbsp)){};
    MCBSP_write16(hMcbsp,aic23data);
    // aic23data = 500;

    // for(temp=300;temp>0;temp-=1)
    // {
    // for(i=0;i<2;i++)
    // {
    // aic23data = 100;
    // MCBSP_write16(hMcbsp,aic23data);
    // delay(temp);
    // aic23data = 0;
    // MCBSP_write16(hMcbsp,aic23data);
    // delay(temp);
    // }
    // }

    //MCBSP_write16(hMcbsp,aic23data);
    }
    }