This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM2707无法识别



按照datasheet参考电路2焊的电路板,在win7下无法识别,显示是未知设备,请问可能是什么原因?

我测了下引脚电压,21脚VDD是3.3V,

2(VCCP)、27(VCCL)、30(VCCR)都是2.6V左右

32(VCOM)是0,23V,这几个电压有没有问题?按照pdf里面的说法,VCOM不是应该是VCCP的二分之一吗?

  • 还是可能你的电路中有问题,你再仔细检查一下电路图和PCB板上的下面几处:

    1. 晶振电路

    2. Pin3、9、10、15、16是否按照推荐的方式设置好了

    3. D+上拉电阻供电是否正确(VDD 3.3V上拉电源,1.5kΩ)

    VCOM电压是应该为VCCP/2,但是如果芯片初始化不成功(例如被PC识别为未知设备),VCOM是没有输出电压的(VCOM是受控的)。