This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5825M: 30W class-D digital input audio amplifier

Part Number: TAS5825M
Other Parts Discussed in Thread: TPA3220

Hi expert,

如下D类功放,帮忙看下是否有合适推荐,谢谢!

1、满足低温-40°C的工业级

2、单声道D类功放,可提供功率30W以上(实际25W),静态电流<16.5ma

3SNR 107dB,噪声级别< 40µVRMSTHD+N 0.03%

4、其他:小封装、EMI优化、支持 32 44.1 48 88.2 96kHz 采样速率

x 出现错误。请重试或与管理员联系。