Part Number: TAS5825MEVM
Other Parts Discussed in Thread: TAS5825M
I have some problems with TAS5825MEVM debugging. Can you help me?
Issue 1: Connection problem: PC -->PPCMB -->TAS5825EVM -->terminal device? If I want to debug the TAS5825M product, do I connect I2C on PPCMB to I2C on TAS5825M or I2C on TAS5825EVM to I2C on TAS5825M?
Issue 2: The power supply problem of the development board: Use Micro-USB to connect the PPCMB with the PC. The blue LED on the PPCMB is always on, but the LED on the TAS5825EVM board is not on. It seems that there is no power supply. I want to know how to make it work normally.
Issue 3: If the first two problems are solved, can it solve the I2C Error error when the PPC3 software connects the device?