Part Number: TAS5825M
在不使用purepath console 3软件的情况下,应该设置那些寄存器使得功放能够对96k采样率的音频数据进行输出
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,寄存器可通过28h来配置。配置完可通过读取FS_MON寄存器确认下是否配置成功。


寄存器读clock fault,fault引脚拉低了吗?寄存器0x78 bit7写1,把clock fault 清零试试。
其他采样率都是正常工作的吧? 事实上,寄存器28h FSMODE即使不手动配置96Khz,默认配置是自动检测采样率的,如果采样率改为96Khz也不会出现问题。
所以原因并不在96Khz设置上,检查下SCLK,您配置的是128fs还是其他?看下SCLK是否不是准确的128fs导致。
您好,抱歉回复晚了。 我建议您申请PPC3 软件,然后使用PPC3进行配置。
我附上一篇如何使用PPC3产生头文件的资料,您可以参考下,希望对您有所帮助。