Part Number: TLV320AIC3007
我们想将从MIC输入采集的声音经过AIC3007数字滤波和EQ后得到20Hz~1000Hz之间的音频数据,MCU不采集数字音频信号,数字信号滤波后直接经DAC到耳机输出。在芯片参考手册上Page0 / Register 107的D3位可以将ADC数字转出到滤波器部分,但是要求在关闭DAC,这样就不能实现我们想要的功能。请问还有别的方式实现ADC到DAC的路径吗吗?如果有,麻烦给一下寄存器配置示例。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TLV320AIC3007
我们想将从MIC输入采集的声音经过AIC3007数字滤波和EQ后得到20Hz~1000Hz之间的音频数据,MCU不采集数字音频信号,数字信号滤波后直接经DAC到耳机输出。在芯片参考手册上Page0 / Register 107的D3位可以将ADC数字转出到滤波器部分,但是要求在关闭DAC,这样就不能实现我们想要的功能。请问还有别的方式实现ADC到DAC的路径吗吗?如果有,麻烦给一下寄存器配置示例。
我们想用到的功能是在Figure 24. Record Only Mode With Digital Processing Path Enabled中,SW_D1闭合、SW_D2状态不重要、DAC Powered Up,然后通过HPOUT能在耳机中听到Analog Input的声音,请问这能否实现?
我试过如下配置,但是没能从耳机中听到声音输出,请看一下是否有哪里设置的不正确:
MIC3L is connected to the left ADC PGA : R17 = 0x0F
MIC3R is connected to the right ADC PGA : R18 = 0xF0
The left ADC PGA is not muted and left ADC PGA Gain 0dB: R15 = 0x00;
The rigth ADC PGA is not muted and right ADC PGA Gain 0dB: R16 = 0x00;
Left AGC is disabled: R26 = 0x00
Right AGC is disabled: R29 = 0x00
Left ADC channel is powered up: R19 = 0x7C
Rigth ADC channel is powered up: R22 = 0x7C
DC dither disabled: R76 = 0x00
Left and right ADC highpass filters disabled, left and right DAC digital effects filters disabled (bypassed), left and right DAC de-emphasis filters disabled (bypassed): R12 = 0x00
The Programmable Filter is connected to ADC output, if both DACs are powered down: R107 = 0x08
The left DAC channel is not muted and gain is 0dB: R43 = 0x00
The right DAC channel is not muted and right is 0dB: R44 = 0x00
Left DAC is powered up, rightDAC is powered up : R37 = 0xD0
DAC Output Switching Control(Left DAC output selects DAC_L1 path, Right DAC output selects DAC_R1 path): R41 = 0x00
DAC_L1 is routed to HPLOUT and volume 0: R47=0x80
DAC_R1 is routed to HPROUT and volume 0: R64=0x80
HPLOUT is not muted and output level control = 0 dB: R51 = 0x0F
HPROUT is not muted and output level control = 0 dB: R65 = 0x0F
旁路掉ADC和DAC,直接PGA输出到驱动端是有输出的,这个之前我们已经多次验证过了。
我的全部寄存器配置如下(用I2C接口从3007里读出来的):
0-3:00 00 00 81
4-7:1c 52 40 8a
8-11:e0 07 00 01
12-15:00 00 00 00
16-19:00 0f f0 7c
20-23:78 78 7c 78
24-27:78 02 00 fe
28-31:00 00 fe 00
32-35:00 00 00 00
36-39:cc d0 00 00
40-43:00 00 00 00
44-47:00 2f 2f 80
48-51:2f 2f 2f 9f
52-55:2f 2f 2f 2f
56-59:2f 2f 07 2f
60-63:2f 2f 2f 2f
64-67:80 9f 00 00
68-71:00 00 00 00
72-75:06 00 00 00
76-79:00 00 00 00
80-83:00 00 00 00
84-87:00 00 00 00
88-91:00 00 00 00
92-95:00 00 c6 0c
96-99:00 00 00 00
100-103:00 00 02 00
104-107:00 00 00 00
p1 0-3:01 7e b6 81
p1 4-7:4a 7e b6 02
p1 8-11:27 02 27 02
p1 12-15:27 7e b4 82
p1 16-19:8f 66 76 aa
p1 20-23:75 3a f3 f4
p1 24-27:c3 50 4b 7e
p1 28-31:b6 81 4a 7e
p1 32-35:b6 02 27 02
p1 36-39:27 02 27 7e
p1 40-43:b4 82 8f 66
p1 48-51:f3 f4 c3 50
p1 52-55:4b 7f ff 00
p1 56-59:00 00 00 00
p1 60-63:00 00 00 00
p1 64-67:00 77 78 88
p1 68-71:88 6e f2 77
p1 72-75:78 88 88 6e
p1 76-79:f2 00 00 00