Other Parts Discussed in Thread: PCM2912A
如题,我做X86的时候,没有出音频接口,现在想利用USB接口转一个音频接口,包括耳机和MIC,但是我在看PCM2707C的时候,感觉PCM2707C只能输出耳机,不能输入MIC。请问想要同时输出两个接口应该怎么做?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: PCM2912A
如题,我做X86的时候,没有出音频接口,现在想利用USB接口转一个音频接口,包括耳机和MIC,但是我在看PCM2707C的时候,感觉PCM2707C只能输出耳机,不能输入MIC。请问想要同时输出两个接口应该怎么做?谢谢!
PCM2707C不支持MIC输入,因为它只是一颗DAC。要同时支持音频输出和MIC输入的,你可以看看PCM2912A。
不需要,windows自带USB声卡的驱动。接到PC的USB端口上会自动识别成USB音频设备并自动安装驱动。
如果是linux的操作系统,需要驱动吗?
另外有无能支持-40~+85℃的工作温度的类似功能的芯片?
Linux不需要专门的驱动,PCM2707C是USB Class Audio,兼容HID协议,只要你的操作系统支持USB Class Audio和HID协议,就不需要任何额外的驱动。
没有-40~+85℃温度范围的,都是-25~+85℃的。
TI工程师,您好,我想实现USB输出转换为IIS信号,同时IIS输入通过USB录音,pcm2707能实现吗?看PDF,输出IIS肯定可以,芯片有IIS的Din管脚,是否能够通过该管脚实现IIS到usb录音,开发产品急用,等您回复,感谢,另有其他推荐的芯片吗?
PCM2070芯片的I2S是给DAC,然后从HP输出,不可以通过I2S输入到USB录音。