请教一下,我在pcm1794数据手册里面看到典型应用电路时输出后用NE5534做IV转换,lt1028做滤波,我自己用的opa2134做IV转换,opa211做滤波,求推荐,使用哪种更好?还有我是做usb声卡,pcm2707用来转i2s,pcm1794用在这上边会不会大材小用?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我觉得没有必要用PCM1794,因为PCM2707是16bit,1794是24bit,PCM1794会受前面的精度限制,信噪比无法发挥出来。
你用PCM2707转出来的I2S外加DAC还不如就用PCM2707内置的DAC。
“请教一下,我在pcm1794数据手册里面看到典型应用电路时输出后用NE5534做IV转换,lt1028做滤波,我自己用的opa2134做IV转换,opa211做滤波,求推荐,使用哪种更好?”
哪种方案好不好除了性能上的考虑,也会有成本等因素的考虑,主要取决于你的应用是偏向于高性能的还是低成本的。高性能的以及追求HiFi音质的可以考虑一下OPA2134以及OPA2604、OPA1612等高性能的运放。低成本的也以参考规格书中使用的NE5534等。
PCM2707的DAC是16位,I2S跟DAC不是一个概念,datasheet上没看到I2S是16位的说法。
实际上很多电路都是用PCM2706/7的I2S接到PCM1794的。