This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AIC3254

 您好!

    我想用AIC3254实现简单的音频对讲功能,甲方MIC1输入,通过 喇叭1输出到乙方,乙方MIC2输入, 通过喇叭2输出到甲,双MIC,双喇叭要求能同时双工通话:
 
1)、电路设计上,能否不通过软件控制,直接实现MIC输入,---OUT输出,解决啸叫?直接用INL1  、INR1分别接MIC1、 MIC2,对应HPL、 HPR分别输出是否可以??还是说需要用两颗AIC3254芯片,各接一个MIC?
2)、如果用MCU配置音频芯片,是否只需要走I2C配置即可,其它的接口,音频接口BCLK\WCLK)可以不用连接(系统不需要实现音频文件的播放),控制?是否还有其它必需要接的关键信号?
 
 
  • 1. AIC3254使用时必须通过I2C配置,并且不支持防啸叫,防啸叫功能需要专门的反馈抑制算法,AIC3254没有这个功能。

    2. 电路上是可以实现你的功能,但不知道你传输的距离有多远?另外,如果你只是实现简单的语音对讲,用不着AIC3254。两个“MIC->前置放大->功放->喇叭”纯硬件电路即可实现。

  • 楼主 您好,我现在也要实现你所说的全双工通话,但是不知道怎么下手,希望您能给我一点帮助,有没有相关的资料