This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
差分放大电路如图所示,采用对输入信号进行5倍衰减,信号源发出15v幅值正弦波,运放采用单5v供电,通过仿真电路可以正常工作,实际工作中会不会损坏放大器?
我实际使用的是OPA1637
您好,
仿真时测试下各管脚最大电压在Absolute Maximum Ratings表格范围内就不会损坏。我看了下电路图没发现哪里有问题,您实际测试有什么问题吗?
谢谢,信号源输出电压摆幅已经超过了电源轨,按照上图电路配置,1、VF3和VF4间的电压最大输入范围在多少才不会损坏运放,应该怎么计算?2、如果按照放大电路配置,R1和R3值互换,VF3和VF4间的电压最大输入范围是多少
大师帮忙解惑一下啊
是否损坏运放是看运放的各管脚电压是否超过了SPEC参数,而不是说前端输入信号的幅值。