This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好:
TAS5707,是20W的数字功放,电视机等home audio里用的比较多,一般需要用到driver的场合不多。
所以TAS5707我们没有对应的driver,需要自行开发。
你说的Porting driver是否是移植?
你好:
我们现有的Linux driver是关于codec的,没有类似于TAS5707的。
但是都是标准的I2C,I2S,你们如果可以开发wolfson的,开发这个应该难度也不大。
但是5707应用到操作系统中,用的真的不多。您可以说一下您的需求,这样方便您选对最合适芯片。
TAS5707对外只有I2S和I2C接口,只要你的操作系统I2C通信这块的driver搞定了,操作TAS5707就是通过I2C函数写相应的寄存器了。datasheet上有详细的寄存器描述及初始化配置说明。
感謝兩位的回覆
TAS5707 是客戶指定的 Chip
客戶本身會有 MCU 拉 I2C 至 TAS5707
而我這邊則是 RT5350 拉 I2S 至 TAS5707
及 UART 至 MCU
謝謝