TI专家你们好!
我使用PCM1794做音频处理,采用单声道模式,发现声音很破,有杂音,沙音等怪怪的现象,就好像声音有残缺或者重叠一样,电路接法如附图,接回立体声模式就很正常,请问是什么原因?是否这种接法有问题?该如何解决?盼复。谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好:
1.我看你的图上面只接了一个通道的滤波器,你提到的单独接两个通道应该是说每个通道分别工作,是吧?如果正常工作,说明芯片和滤波器起作用了。
2.看你的图,是把连个通道并起来接成的MONO模式。但是我们的datasheet上并没有推荐这样接,我们推荐的MONO模式,请参加page 22,figure 26,balance的接法。
3.PCM1794是电流型的DAC,输出是电流,直接把输出的两路并起来,输出的两个通道阻抗不是完全一致,就会造成回流。
4.还有你需要看一下,两个通道输出的是同向还是反向,同向的顾虑如3,如果是反向,自然也不能并联。
你好:
这样的话,我觉得PCM1794输出的是电流,如果两个通道不匹配,是有机会并联引起噪声的。
我的建议是试试输出串个电阻,调试一下电阻值,待两个通道的输出匹配后,再并联。
请教下TI专家,我看了TI官方的spec,感觉OPA1612,OPA1611与OPA2211,OPA211的参数差不多,没有太大的差别,在这里想问下,PCM1794后面的IV+LPF用OPA1612+OPA1611组合好一些还是用OPA2211+OPA211组合相对更好一些?能详细谈谈各自的优缺点吗?
你好:
音频比较关注THD+N和SNR,所以对于运放的选取,比较关注的参数有THD,noise等,可以从这两个角度比较一下两种组合。