This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

【原创】失调电压问题

失调电压,又称输入失调电压,Input Offset Voltage, 记为U1,一个理想的运放,当输入电压为0时,输出电压也应为0。但实际上它的差分输入级很难做到完全对称。通常在输入电压为0时,存在一定的输出电压。

解释一:在室温25℃及标准电源电压下,输入电压为0时,为使输出电压为0,在输入端加的补偿电压叫做失调电压。

解释二:输入电压为0时,输出电压Vo折合到输入端的电压的负值,即VIO=- VO|VI=0/AVO

输入失调电压反映了电路的对称程度,其值一般为±1~10mV

由例图得出输入失调电压 计算公式:

U1 = R1/(R1+Rf)·Uo

测试失调电压的方法

运放输入失调电压测试只要将运放连接成差分放大电路(也称减法电路),再将两个输入端短接之后接地即可。

为了方便测量,可设置较大的增益,如1001倍,输出电压除以1001就是输入失调电压。

可以采用下述电路测量:

取RF=R3=100kΩ,R1=R2=100Ω,将Ui1和Ui2同时接地,Uo/1001就是输入失调电压。