PCM1802工作于Master mode (384 fS),系统时钟为18.432MHz,Data Format为I2S, 24-bit,用示波器测得FSYNC(96kHz), LRCK(48kHz), DOUT均有信号输出,唯独BCK一直保持高电平,正常情况下应输出3.072MHz信号才对啊?还望哪位大侠帮忙解决下,万分感谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好:
1.PCM1802是纯硬件模式,改MODE0和MODE1即可更改模式,没有别的寄存器设置。但是BCK没有输出,所以我建议先检查一下硬件,原理图,PCB上有无短路等。
2.如果确认无误,看是否方便改一下模式,例如改为256fs master模式,看是否还存在这个情况。