This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tlv320aic3254evm-u的pps使用问题

各位秀才,进士,举人好,我最近在使用3254evm-u调试minidsp的aec功能遇到以下问题:

 首先描述下我的平台:目前通过3254-cs软件可以正常配置evm板,通过在evm上插上麦克风(mic)和耳机(headphone)可以实现收听pc上的mp3和pc的录音机收录麦克风收到的声音。

问题1:我现在使用的pps版本是"setup_PurePath_Studio_Portable_Audio_MiniDSP_v5.95_build1_rev28655.exe",在其他相关的pps手册上看到firmwork中有个3254_aec的模块,但是我的pps上找不到这个模块,是我模块不全,还是在这版本的pps里面已经将aec模块合成到3254模块里面了。大神可否上传个最新的库文件夹给我啊~~感激不尽。

问题2:我首先用cs把3254evm的hp和mic端口都测试正常以后,打开pps调用example文件夹中的任意工程,然后再点download到evm之后,mic和hp的功能就失效了,查找了支持社区的相关内容,有的进士提出cs要和pps配合使用,我想知道应该怎么配合调试,pps的指导手册里没有找到相关论述。