This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我在用TPA3110时,当输入为1Khz音频信号,在输入信号工作时,SD信号拉低,会听到POP音,如果将输入信号停止,然后SD信号拉低,则没有POP音。因为通常的关机时序都是先关SD功放,然后撤销输入信号。而且在掉电状态下系统无法做到先撤销输入信号,再将SD信号拉低。
在这种情况下如何消除POP音?--谢谢
你好:
请问你的功放输出是BTL还是SE接法?
可以尝试在输出端加个mute电路,先mute,再SD,避免SD时的POP。
Flora,你好
是BTL output, SE input接法. TI 有没有建议的输出Mute电路供参考?谢谢