我手上没有LM1875了,现在我需要驱动10w的高音喇叭,LM3886信不信,会不会把喇叭烧了?如果可以,应该怎样做,大神求教。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好:
您是什么应用,选用class AB的功放,需要高保真吗?
烧坏喇叭主要是因为电流过大,也即使输出功率过大。
现在使用LM3886,供电电压低一点,或者前级输入的音频小一点,注意不让负载的输出功率过大,就不会少坏喇叭。
感谢您的回答,需要高保真,我做一个2.1的有源电子三分频音箱,10w的喇叭,用lm3886做功放,lm3886用多大的电压供电最好,才不会烧喇叭
我做的正负25v的电源,有30mv的纹波,这对功放有木有影响?
你好:
1.电源电压是+/-25V,那么输出信号的电压峰值最大为25VPK,有效值为25/1.414=17.6Vrms,也就是输出最大为17.6Vrms,如果是8ohms的喇叭,输出功率最大为:
P=17.6*17.6/8=35W。也就是说当前供电电压下最大输出功率为35W,而喇叭最大承受功率只能为10W。
2.反过来讲,10W输出功率,8ohms喇叭对应的电压有效值为8.9Vrms=12.6VPK。也就是说电源的供电电压要大于+/-12.6V,但是不能太大,太大就起不了限制的作用;太小电源,不够用。输出信号不能超过12.6V(这需要你匹配Gain,限制前级的输入信号即可)。