为什么我们买的DEMO板 在测试频响的时候只到6KHZ(-3DB),然后我们做的产品出来也是到6K,这是什么原因,我们做过一些测试,在进入PM1808之前的信号是到20K以上的,进了ADC,从5715出来后就只能到6K。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好:
你应该是用GDE初始化的吧,请检查有没有开EQ?还有采样频率是多少?
我们的demo板上用的LC滤波器参数是15uH+0.68uf,截止频率为50K,如果你用PCM1808输入的话,根据奈昆斯特采样定律,PCM1808输出的应该是0.5fs.
所以整体下来应该是0.5fs.
跟负载没关系。那你的频响大概在24K左右。
我们EVM频响不可能只有6K,应该是设置或者测量问题。
你用什么测试的频响,证明只有6K?
我们是用AP测试的,我们也做过TAS5707,TAS5508,这两个做的都是可以到20K以上的,我认为我的测试方法是没有问题的。