This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3120的D/A问题

将C5515与这个codec连接,5515通过I2C对codec寄存器进行配置,DSP生成正弦波通过DA恢复出来,现在就配置了D/A这一块,配置是参照datasheet配置的,用示波器看时钟和数据都有,但是用示波器查看输出端的波形时,只有插上耳机才会有输出波形,不插耳机,看不到输出波形,并且插上耳机,并没有响声。请问这是什原因,谢谢!

  • 亲;是在DA口量的还是输出口量的?耳机口内是否有开关?频率是多少?

  • 亲,是在DA的输出口测量的,采样频率是44.1k,DSP给codec发送的信号频率是1k,插上耳机后,也在耳机那里测量也有信号,拔掉耳机测量就没有信号了!下面是寄存器的配置:

    AIC3120_rset( 0, 0x00 ); //选择PAGE 0
    AIC3120_rset( 1, 0x01 ); //启动软件复位

    /*程序时钟设置,Program PLL clock dividers P, J, D, R (if PLL is used)*/
    AIC3120_rset( 27, 0x0d ); //mode is i2s, word length is 16, MASTER mode
    AIC3120_rset( 28, 0x00 ); // Data ofset = 0
    AIC3120_rset( 4, 0x03 ); //PLL_clkin = MCLK,codec_clkin = PLL_CLK
    AIC3120_rset( 6, 0x07 ); //J = 7
    AIC3120_rset( 7, 0x02 ); //D = 560, D(13:8) = 10
    AIC3120_rset( 8, 0x30 ); //D(7:0) = 00110000
    AIC3120_rset( 30, 0x8C ); // For 32 bit clocks per frame in Master mode ONLY
    AIC3120_rset( 5, 0x91 ); //启动锁相环(如果使用锁相环),PLL Power up, P = 1, R = 1
    EZDSP5515_waitusec(10000); //Wait for PLL to come up
    AIC3120_rset( 13, 0x00 ); //DOSR = 128, DOSR(9:8) = 0
    AIC3120_rset( 14, 0x80 ); //DOSR(7:0) = 128
    AIC3120_rset( 11, 0x85 ); //Power up NDAC and set NDAC value to 5
    AIC3120_rset( 12, 0x83 ); //Power up MDAC and set MDAC value to 3
    AIC3120_rset( 18, 0x85 ); //Power up NADC and set NADC value to 5
    AIC3120_rset( 19, 0x83 ); //Power up MADC and set MADC value to 3
    AIC3120_rset( 20, 0x80 ); //AOSR for AOSR = 128 decimal or 0x0080 for decimation filters 1 to 6


    /*DAC ROUTING and Power Up*/
    AIC3120_rset( 0, 0x00 ); //选择PAGE 0
    AIC3120_rset( 60, 0X07 ); //DAC Processing PRB_P7, change the processor as needed
    AIC3120_rset( 116, 0x00);
    AIC3120_rset( 68, 0x00 );
    AIC3120_rset( 65, 0x00 );
    AIC3120_rset( 0, 0x01 ); //选择PAGE 1
    AIC3120_rset( 33, 0x4E ); //De-pop, Power on = 1.22s, Step time = 3.9 ms
    AIC3120_rset( 31, 0xD4 ); //HPL and HPR Power up, current limit, CM = 1.65V 0xD4
    AIC3120_rset( 35, 0x40 ); 
    AIC3120_rset( 40, 0x0E );  //HPL and HPR unmute and gain 0db
    AIC3120_rset( 36, 0x00 ); 
    AIC3120_rset( 37, 0x00 );
    AIC3120_rset( 0, 0x00 ); //选择PAGE 0
    AIC3120_rset( 60, 0x0B );
    AIC3120_rset( 0, 0x08 );
    AIC3120_rset( 1, 0x04 );
    AIC3120_rset( 0, 0x00 ); //选择PAGE 0
    AIC3120_rset( 63, 0xD6 );
    AIC3120_rset( 64, 0x00 );

  • 你好:

    你看到的波形是什么样的?1K的正弦波?如果能看到那就证明HP有输出,耳机听不到说明耳机端的接线有问题。

    先确认耳机端有没有输出在看下原理图。

  • 是1k的正弦波,关键是耳机插上才有波形,不插耳机没有波形,不知道这是什么问题。

  • 你好:

    检查下你耳机的接线,或上传耳机部分的原理图,输出部分肯定有问题.

  • 你好:

          我再次检查了耳机的接线,确实是耳机接线没接对,谢谢!