Other Parts Discussed in Thread: TPA6130A2, TPA6133A2
因TPA6133A2在国内使用不是很多,货源也必较少。因此想用TPA6130A2代替,但是这个的音量是I2C控制的,而我需要做的产品不需要CPU控制,只要硬件控制就好了。
问题1 TPA6130A2如果不需要I2C功能,是否可以将I2C的两个引脚悬空。
2.如果将I2C两个引脚悬空,该IC是否是最大音量,而且长期使用和多次通电IC是否依然保持最大音量。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sir,
TPA6133 模拟部分性能和TPA6130 是一样的, 如果不想要CPU控制, 那就建议用TPA6133. TPA6130 HW默认状态是mute的, 必须要I2C 控制才能正常工作.
如果输出功率不需要那么大,可以考虑TPA6132. 这一颗用的人很多.
Best Regards
Fabian Zhang