大家好,问一个关于DIR9001芯片的问题,不久前做了这个电路,DIR9001接收数字信号转成I2S信号给PCM1794,对于DIR9001我使用了外部的有源24.576MHz晶振,现在,我输入了同轴信号,测试I2S输出信号,SCK,LRCK,BCK信号都对,但是DOUT信号没有,RXIV是有输入信号的,是不是DIR9001没有锁住呢?第二,只要输入同轴信号,D11就亮了,DIR9001手册里写到,只要锁住信号,并且没有发现校验错误ERROR pin就是低电平,这又是怎么回事呢。第三,我想问使用了确定频率的外部晶振,那么对输入同轴数字信号有什么要求,对于输出LRCK=96KHz的信号,难道一定要输入96K的信号么,我看到过如果不使用内部PLL,而使用外部晶振是基于一种重采样的原理?。希望得到大家的帮助,在此先谢谢大家了!