This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于TLV320AIC3204EVM音频接口输入和输出的问题

我对音频输入和输出不太懂,3204三组输入IN1L,IN1R和IN2L,IN2R,IN3L.IN3R,是否既能麦克风输入,又能线路输入?比如我连接电脑或者手机的耳机接口,按照开发板给定的外围电路,是否能把声音的模拟信号导入到3204,另外LOL.LOR连接电脑的麦克风口或者手机,是否能把声音的模拟信号导入到电脑或者手机。

比如我把手机和3204开发板通过一个4芯耳机相连,通过设计一些程序,让手机在处于通话状态的情况下,将手机的模拟声音信号进行模数-数模转换,让我能听到转换后的模拟信号;而我的声音经过麦克风,导入到3204,经过模数-数模转换,传给手机,让手机另一头的人能听到我说的话。整个过程,是否可以实现,会有什么问题吗?

  • 你好:

    1.AIC3204的三组输入确实既能MIC输入也能线路模拟输入。到那时MIC输入,需要接MICbias。EVM板上只在LIN3接了MICbias,所以只有LIN3能接MIC,其余接线路输入。

    2.电脑或者手机口的耳机接口,接EVM板上的LIN,可以将模拟声音给3204,通过ADC,可以得到数字信号,这就是录音。将模拟信号导入手机,你直接把手机打开录音功能就好了,手机里也有codec,录音过程和这个一样。

    3.声音经过MIC给AIC3204,不能传数字信号给手机,因为手机没有开放I2S接口和EVM相连。

  • 你好:

    关于第二点,将模拟信号导入手机,如果我想把经过3204数字-模拟后的音频信号导入手机,是应该通过HP OUT给手机,还是应该通过LINE OUT给手机?

    因为我对手机内部麦克风接口的连接不了解,手机的麦克风接口应该自带偏置电压,如果将3204转换后的音频信号通过手机麦克风接口导入手机,这个偏置电压是否有影响