This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,若I/V变换电路一样,请使用同样的供电电压。
反馈电阻560,中心电流6.2mA,则第一级I/V的输出为3.8V左右,输出电流7.8mA pp,则输出电压为5.6V最大,用5V供电,肯定削波啦。
如果要保证这颗IC的超高性噪比,请保证她的幅度。若一定要使用5V供电,请使用boost芯片将电压升上去。
谢谢
对于你的系统,左边会先失真,你可以可以输出正弦波,然后去观测左边节点的电压。
1.2V是静态的时候?两个都是1.2V?