Other Parts Discussed in Thread: TLV320AIC3254, CC3200
如题
目前使用STM32与TLV320AIC3254进行数据传输,TLV320AIC3254是从机,查看I2S波形发现MCLK波形不连续,是断断续续的,这是正常的吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TLV320AIC3254, CC3200
如题
目前使用STM32与TLV320AIC3254进行数据传输,TLV320AIC3254是从机,查看I2S波形发现MCLK波形不连续,是断断续续的,这是正常的吗?
Hi James,
What is the codec clk source you are using now? from I2S BCLK or MCLK? Actually, AIC3254 can works well without MCLK.
Best Regards
Fabian Zhaang
工作在从机模式下也可以不用MCLK?使用BCLK作为参考吗?
你好:
是的,如果你无法保证你的MCLK连续,那么可以不要MCLK,使用BCLK做时钟来源,但是要保证你的BCLK足够的快,不能太小,最小要是512K。
然后选择PLL_CLK=BCLK,enable PLL,在配置R,J,D等参数。
你好:
请参见page1 register 51, 这个模式应该是对应的register 51描述的几种配置。
你好,
FLORA , 我是艾电创新的LANDY,目前用CC3200+3254时,录播声音没有问题,可是在实时
的时候,声音就变调了,我有把MCLK和BCLK短路,APP跑的是单声道 16K ,我这边是双声道,
不知道要如何解决?请帮忙一下。