Other Parts Discussed in Thread: TPA6130A2
In the datasheet of TPA6130A2,
TA Operating free-air temperature range is –40°C to 85°C
TJ Operating junction temperature range is –40°C to 125°C
And in page 6 there are two parameters of Thermal shutdown, 1. Threshold 180 °C 2. Hysteresis 35 °C
这2个参数代表什么含义?
Thermal A 1 on this bit indicates a thermal shutdown was initiated by the hardware. When the temperature
drops to safe levels, the device will start to operate again, regardless of bit status. This bit is
clear-on-read.
当温度降到正常值,IC会重新启动,(不管寄存器的值);
温度降下来了,寄存器的值是否会自动变化?